DTL_CIP_APPLICATION_UNREGISTER parameters
reg_id
is the handle to the application registration which was returned by DTL_CIP_APPLICATION_REGISTER.timeout
is the maximum time (in milliseconds) to wait for the registration to be removed.Provide Feedback