RSLinx Classic Single Node

RSLinx Classic Single Node includes the required functionality to supply communication services for all Rockwell Software products. OPC and DDE interfaces are supported, but to only one device. It does not support applications developed for the RSLinx Classic C Application Programming Interface (API) or direct drivers in HMI applications. RSLinx Classic OEM or higher is required for these application types.
RSLinx Classic Single Node is used for the following:
  • Data acquisition using OPC or DDE to only one device. This includes clients such as RSView32, Microsoft Office, Visual Basic, and web pages.
  • Ladder logic programming using RSLogix products.
  • Network and device configuration and diagnostics using RSNetWorx.
  • Configuring 1756-ENET, 1756-DHRIO, and the Redundancy modules (for example, 1756-RM, 1756-RM2).
  • Upgrading firmware using ControlFlash.
  • Browsing networks and getting device information such as firmware revision.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal