RSLinx Classic OEM

RSLinx Classic OEM includes the required functionality to supply communication services for all Rockwell Software products. OPC and DDE clients are supported for any number of devices. It also supports applications developed for the RSLinx Classic C Application Programming Interface (API).
RSLinx Classic OEM version 2.2 and previous versions only support AdvanceDDE. RSLinx Classic version 2.3 and subsequent versions support all DDE types except FastDDE.
RSLinx Classic OEM is used for the following:
  • Data acquisition using OPC or DDE to any number of devices. This includes clients such as RSView32, Microsoft Office, Visual Basic, and web pages.
  • Ladder logic programming using RSLogix products.
  • Network and device configuration and diagnostics using RSNetWorx.
  • Configuring 1756-ENET, 1756-DHRIO, and the Redundancy modules (for example, 1756-RM, 1756-RM2).
  • Upgrading firmware using ControlFlash.
  • Browsing networks and getting device information such as firmware revision.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal