RSLinx Classic Lite

RSLinx Classic Lite provides the minimum functionality required to support RSLogix and RSNetWorx. This version is not commercially available, but is bundled with products that require only direct access to the RSLinx Classic network drivers. This version does not support OPC, DDE, or the published RSLinx Classic C Application Programming Interface (API).
RSLinx Classic Lite is used for the following:
  • Ladder logic programming using RSLogix products.
  • Network and device configuration and diagnostics using RSNetWorx.
  • Configuring 1756-ENET, 1756-DHRIO, and the Redundancy modules (for example, 1756-RM, 1756-RM2).
  • Upgrading firmware using ControlFlash.
  • Browsing networks and getting device information such as firmware revision.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal