RSLinx Classic OPC servers

RSLinx Classic provides the following types of OPC servers:
  • RSLinx OPC Server
    A 32-bit or 64-bit OPC DA server connection for OPC DA clients running on the same workstation.
  • RSLinx remote OPC Server
    A 32-bit or 64-bit OPC DA server connection for OPC DA clients running on a different or remote computer.
  • RSLinx Local OPC Server
    A 64-bit OPC DA server connection for 64-bit OPC DA Clients running on the same workstation using the RSLinx Classic Single Node or OEM edition activations.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal