Toolbar

The toolbar contains shortcuts to several commonly used RSLinx Classic functions. Each toolbar button is a graphical representation of a command that is also available from the RSLinx Classic menu bar. The following items appear on the RSLinx Classic toolbar.
RSLinx Classic Linked Icons PNG FIle Template
Icon
Menu Selection
Description
RSLinx Classic Linked Icons PNG FIle Template
File > Open Project
Displays the currently defined projects and allows you to open a DDE/OPC project. You can also press Ctrl+O to display the Open DDE Project dialog box.
RSLinx Classic Linked Icons PNG FIle Template
Communications > RSWho
Opens an additional instance of RSWho (one instance is opened by default each time you open RSLinx Classic.
RSLinx Classic Linked Icons PNG FIle Template
Communications > Configure Drivers
Displays the currently configured RSLinx Classic software drivers and allows you to add additional drivers for use with your hardware devices.
RSLinx Classic Linked Icons PNG FIle Template
Communications > Driver Diagnostics
Displays a list of currently configured drivers and provides the option to view diagnostic information for each driver.
RSLinx Classic Linked Icons PNG FIle Template
Edit > Copy DDE/OPC Link
Provides the ability to create a DDE/OPC link between RSLinx Classic and a client application such as Microsoft Excel.
RSLinx Classic Linked Icons PNG FIle Template
DDE/OPC > Topic Configuration
Allows you to create and modify a DDE/OPC topic, which is a specific path to a processor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal