Status bar
The status bar at the bottom of the RSLinx Classic screen provides information about the current status of your system.

The left area of the status bar is used to pass messages to the user. For example, when you scroll through the items on the menus, a brief description of the function of that menu item appears in this area of the status bar.
The right area of the status bar displays:
- CAP, which is highlighted if the Caps Lock key on your keyboard is toggled for all caps.
- NUM, which is highlighted if the Num Lock key on your keyboard is set to enable the numeric keypad on your keyboard.
- SCRL, which is highlighted if the Scroll Lock key on your keyboard is set.
- The current date from your computer's system clock/calendar.
- The current time from your computer's system clock/calendar.
Provide Feedback