Setting the local language
To select the language to run with RSLinx Classic, click
Start
and select Programs > Rockwell Software > RSLinx > RSLinx Classic Launch Control Panel
. The Select Language
drop-down list box contains all the languages supported in the current version of RSLinx Classic.
TIP:
If RSLinx Classic is running, this drop-down list box is disabled.
If RSLinx Classic is running as an application, the language displays as the setting in the Windows
Control Panel
. However, Windows can only configure the default language when the operating system is installed. Therefore, if RSLinx Classic is running as a service
, you must change the language using the control on the RSLinx Classic Launch Control Panel
.If you select another language, RSLinx Classic displays in that language regardless of any system or user language setting. If you select
System Default
, RSLinx Classic displays in the default language set in the Windows Control Panel
.Provide Feedback