List control (right pane in the RSWho)
The right pane of the
RSWho
is the list control, which shows all members of a collection. A collection is a network, or a device that is a bridge. Right click in the list control and choose a view option of large icons or details. You can also right click a supported device to select Station Diagnostics, Configure DDE Topic, or other supported services for that device.Provide Feedback