Control bar

The control bar of the
RSWho
contains the following items:Item | Description |
|---|---|
![]() | The Autobrowse check box is selected by default.
|
![]() | The Refresh button is available if you clear the Autobrowse check box. Clicking the Refresh button instructs RSWho to perform one browse cycle of the selected device or network. Since clicking the button only performs one browse cycle, you may need to click multiple times to discover everything on the network. |
The EDS file auto-upload button indicates whether the EDS files automatic upload and registration function is enabled. If you turn on the EDS file auto-upload button, RSLinx Classic automatically uploads and registers EDS files of unrecognized online devices upon device and network browsing. By default, the button is turned off, and the automatic upload and registration function is disabled.For more details, see Automatically upload and register EDS files of devices in RSWho. | |
The Show large icons button indicates how devices and networks show in the list control (right pane) in the RSWho . If you click the Show large icons button, devices and networks show as large icons. By default, the button is turned on, and devices and networks show as large icons. | |
If you click the Show details button, devices and networks in the list control (right pane) show in a list. You can view device details such as Address, Device Type, Online Name, and Status. | |
Status | The status of device and network browsing. Tip: Be patient when browsing some networks, such as through a 1785-KA, as it may appear that no devices exist, but the update is only being delayed as RSWho checks all possible station addresses. |
Provide Feedback