Options, DDE/OPC Tab
Select
DDE/OPC > Options
or View > Options
to display the Options
dialog box which contains the DDE/OPC
tab. The DDE/OPC
tab provides these abilities:- Log communication errors
- Display addressing errors
- Use English language for DDE conversationsCF_TEXT based floating point uses English floating point separators with this selected, and the language specific separators if not selected. If the machine's language is changed, RSLinx Classic will use the new language unless this is selected.
- Save communication errors to a fileYou can selectBrowseto specify the log file path.
- Enable Automatic Client Connection CleanupWhen requested by an OPC client, RSLinx Classic will allocate internal threads and open connections to a controller. However, RSLinx Classic is not notified when an OPC client stops communicating, causing the connection and thread resources to remain allocated. These leftover resources could impact normal operation, especially in a large heavily loaded system. By enabling Automatic Client Connection Cleanup, RSLinx Classic will perform a resource check at the interval that you specify to determine if connections and threads can be closed.
Provide Feedback