Menu bar - View
RSWho
- Opens an additional instance of RSWho (one instance is opened by default each time you open RSLinx Classic). You can also click the RSWho toolbar button to open an instance of RSWho.Event Log
- Views system occurrences such as drivers starting and stopping successfully.Options
- Selects RSLinx Classic settings such as toggling the Status Bar and running RSLinx Classic as a service.Provide Feedback