Menu bar - File

Open Project
- Displays the currently defined projects and allows you to open a DDE project. You can also click the Open DDE Project toolbar button or press Ctrl+O to display the Open DDE Project dialog box.
Select Default Project
- Displays the currently defined projects and allows you to select the project to be active when you start RSLinx Classic. If you have not created a project, a default project is automatically created and selected.
Compact Harmony
- Removes all the existing topology files that are stored in RSLinx Classic.
Edit
- Terminates all DDE links and exits RSLinx Classic.
Exit and Shutdown
- Terminates all DDE links and exits RSLinx Classic. This menu item is only available when running RSLinx Classic Services.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal