Menu bar - DDE/OPC
Topic Configuration
- Creates and modifies a DDE/OPC topic, which is a specific path to a processor. You can also click the Topic Configuration toolbar button to display the DDE/OPC Topic Configuration dialog box.Alias Topic Configuration
- Creates a "virtual" or "redundant" topic that you can use to reference other topics.Active Topics/Items
- Displays a window with the topic name and item description for each active DDE topic.Communication Events
- Displays information on any DDE error messages logged while running RSLinx Classic with DDE compliant programs.Optimized Packets
- Displays the optimized network traffic for all DDE Topics.Server Diagnostics
- Displays RSLinx Classic diagnostic information when DDE links exist.DDE Client Diagnostics
- Displays diagnostic information for the client application that contains DDE links to RSLinx Classic.OPC Group Diagnostics
- Displays diagnostic information for RSLinx Classic and the client application that contains DDE links to RSLinx Classic.Update ControlLogix Tag Info
- Displays a list of current DDE/OPC ControlLogix topics and provides the ability to merge new tags into the list.Options
- Selects RSLinx Classic settings such as toggling the Status Bar and running RSLinx Classic as a service.Provide Feedback