Menu bar - Communications

RSWho
- Opens an additional instance of RSWho (one instance is opened by default each time you open RSLinx Classic). You can also click the RSWho toolbar button to open an instance of RSWho.
Configure Drivers
- Displays the currently configured RSLinx Classic software drivers and allows you to add additional drivers for use with your hardware device. You can also click the Configure Drivers toolbar button to display the Configure Drivers dialog box.
Configure Shortcuts
- Creates a shortcut to a remote network.
Configure Client Application
- Connects configured and running RSLinx Classic drivers to legacy INTERCHANGE C API xKT:0 labels.
Configure CIP Options
- Configures how PCCC requests are sent over networks that use the CIP protocol and to set up messaging connections for ControlLogix processors.
Configure Gateway
- Enables the RSLinx Classic Gateway. When you choose to enable the RSLinx Classic Gateway, the changes will not take effect until you shut down and then restart RSLinx Classic. The Configure Gateway menu option only appears when running the RSLinx Classic Gateway. It does not appear if you are running RSLinx Classic Lite, RSLinx Classic OEM, or RSLinx Classic.
Driver Diagnostics
- Displays a list of currently configured drivers and provides the option to view diagnostic information for each driver. You can also click the Driver Diagnostics toolbar button to display the Driver Diagnostics dialog box.
CIP Diagnostics
- Displays CIP Dispatching, Messaging, and Connections diagnostic information.
Gateway Diagnostics
- Displays diagnostic information for the RSLinx Classic Gateway. The Gateway Diagnostics menu option only appears when running the RSLinx Classic Gateway. It does not appear if you are running RSLinx Classic Lite, RSLinx Classic OEM, or RSLinx Classic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal