Device Properties

The
Device Properties
dialog box displays specific information about the selected device, such as name, vendor, product type and code, revision and serial number, and any fault information present when browsing the device.
To display the
Device Properties
dialog box, right-click on a device in
RSWho
and select
Device Properties
.
TIP: Properties are not available in RSLinx Classic for all devices. If the Device Properties selection does not appear when you right-click a device in
RSWho
, properties are not available for the selected device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal