Delete a driver in RSLinx Classic Gateway

To delete a driver in RSLinx Classic Gateway, no RSLinx Classic clients can be connected. If you need to delete a driver, but cannot shut down all RSLinx Classic clients:
  1. Select
    Communications > Configure Gateway
    from the RSLinx Classic main menu.
  2. From the
    Configure RSLinx Classic Gateway
    dialog box, clear the
    Enable RSLinx Classic Gateway
    checkbox to disable the
    RSLinx Classic Gateway
    .
  3. Click
    OK
    to close the dialog box.
  4. Exit and restart RSLinx Classic.
  5. Select
    Communications > Configure Drivers
    .
  6. From the
    Configured Drivers
    list, select the desired driver and click
    Delete
    .
  7. Click
    Close
    to close the dialog box.
  8. Select
    Communications > Configure Gateway
    .
  9. Select the
    Enable RSLinx Classic Gateway
    check box to enable the
    RSLinx Classic Gateway
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal