Check the DH+ interface group box
The Channel A (or B) Diagnostics tab shows the current state of the DH+ Interface object and any items affecting its state. Normal states for these items are:
DH+ Interface object - Normal
DH+ entry - Run
If you see
Waiting
as the current state, the front display on the module shows CNFG FALT
for that channel. If the state is Waiting
, one or both of the following shows in the Items Affecting State
dialog box:If you see: | Do this: |
DH+ object |
|
Routing Table |
Provide Feedback