Ethernet connection manager diagnostics
Statistics
Field | Description |
Requests | Number of open/close connection requests this module has received. |
Format Rejects | Number of open/close connection request this module has rejected because the request was not formatted correctly or because some parameter value was not within a supported range of values. |
Resource Rejects | Number of open connection requests this module has rejected because the module did not have enough resources (buffers, link bandwidth, or CPU utilization) to honor the request. |
Other Rejects | Number of forwarded open/close connection requests a module rejects. |
Timeouts | Number of connections not explicitly closed by the connection originator, but closed by this module because they were not being used. |
Provide Feedback