IP address ranges overlap

The IP address of one of the Ethernet ports resides within the IP address range of another Ethernet port. This error can occur when the EtherNet/IP Mode is configured for Dual-IP and the Subnet parts of the IP addresses on the Ethernet ports overlap.
The IP address and Subnet mask values that you assign to an Ethernet port establish an IP address range for the port. The Subnet mask value is used to establish the Subnet part of the IP address.
Here is an example of IP address ranges that do not overlap.
Port Number
IP Address
Subnet Mask/Network Mask
IP Address Range (Low to High)
A1
192.168.1.5
255.255.255.0
192.168.1.1…192.168.1.254
A2
192.168.2.1
255.255.255.0
192.168.2.1…192.168.2.254
Here is an example of IP address ranges that overlap.
Port Number
IP Address
Subnet Mask/Network Mask
IP Address Range (Low to High)
A1
192.168.1.5
255.255.252.0
192.168.0.1…192.168.3.254
A2
192.168.2.1
255.255.255.0
192.168.2.1…192.168.2.254
Change the IP address and/or Subnet Mask so there is no overlap of IP address ranges.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal