Browsed Device Downstream in Dual IP mode and DLR mode

If the device supports IP mode change, when the device is browsed, the downstream bus will appear differently for devices configured in Dual IP mode and Linear/DLR mode.
Device is configured in Dual IP mode
  • If you connected to the device from its USB connector, then the following downstream busses should be shown:
    • Backplane
    • A downstream Ethernet bus
    • A second downstream Ethernet bus
  • If you connected to the device from its Ethernet connection, then the following downstream busses should be shown:
    • Backplane
    • USB bus if connected
    • A downstream Ethernet bus
Device is configured in Linear/DLR mode
  • If you connected to the device from its USB connector, then the following downstream busses should be shown:
    • Backplane
    • A downstream Ethernet bus
  • If you connected to the device from its Ethernet connection, then the following downstream busses should be shown:
    • Backplane
    • USB bus if connected
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal