ControlNet connection manager diagnostics

Statistics
Field
Description
Requests
Number of open/close connection requests this module has received.
Format Rejects
Number of open/close connection request this module has rejected because the request was not formatted correctly or because some parameter value was not within a supported range of values.
Resource Rejects
Number of open connection requests this module has rejected because the module did not have enough resources (buffers, link bandwidth, or CPU utilization) to honor the request.
Other Rejects
Number of forwarded open/close connection requests a module rejects.
Timeouts
Number of connections not explicitly closed by the connection originator, but closed by this module because they were not being used.
Connection statistics
Field
Description
Total Connections
Total number of connections supported by this module.
Connections Used
Number of connections currently open to or open through this module.
Connection Utilization Graph
Shows the percentage of connections used out of the total connections supported by this module.
Buffer statistics
Field
Description
Max Buffer Size
Total number of bytes that the module design has reserved for use by connections.
Size Remaining
Number of bytes currently unallocated to connections.
Buffer Utilization Graph
Shows the percentage of buffer currently allocated to connections out of the total number of bytes that the module design has reserved for future use by connections.
CPU statistics
Field
Description
CPU Utilization
Amount of time currently being spent to support the existing connections and the background processing of the module.
CPU Utilization Graph
Amount of time currently being spent to support the existing connections and the background processing of the module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal