CNB port diagnostics — network configuration
Diagnostic Counter | Description |
Network Update Time | Repetitive time interval in which data can be sent on the ControlNet network. |
Scheduled Max Network Addr | Node with the highest network address that can use scheduled time on a ControlNet link. |
Unscheduled Max Network Addr | Node with the highest network address that can use unscheduled time on a ControlNet link. |
Network Address | Node's address on the network. |
Provide Feedback