Configure chassis size
To configure the chassis size of a 1734-ACNR or 1734-AENT, perform the following steps:
- In theChassis Size In Modulefield, type the size of the chassis in the 1734-ACNR or 1734-AENT.TIP:For connections to work properly, set the chassis size to the number of I/O modules plus the adapter. For example, if you have one I/O module present, set the Chassis Size In Module size totwo.
- In theModify Chassis Sizetext box, select the actual chassis size.
- When complete, clickOK.
Provide Feedback