ControlLogix routing

The ControlLogix routing protocols use the
source routing
model. That is, the source of a message (for example, a MSG instruction in a programmable controller or RSLinx Classic DDE topic) specifies the full route to be taken by that message. This has two significant benefits:
  • You do not need to configure routing tables in the
    bridging
    module, which greatly simplifies maintenance and module replacement.
  • You maintain full control over the route taken by each message, which enables you to select alternative paths for the same end device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal