Valid station addresses
The station address field in a driver configuration dialog box is for the address of the computer, on which RSLinx Classic and the driver are installed. The type of network the communication channel is determines valid addresses.
Network Type | Station Address | Valid Entries |
DH+ | physical station number | 0-77 (octal) |
DH485 | physical station number | 0-31 (decimal) |
TCP/IP | mapped station number | 0-255 (decimal) |
ControlNet | physical network address | 1-99 (decimal) |
DeviceNet | physical network address | 0-63 (decimal) |
The maximum network address may be limited by the network configuration for ControlNet.
Provide Feedback