Remove a shortcut

Removing a shortcut in RSWho does not delete the shortcut. The only valid way to delete a shortcut is by selecting it in the Configure Shortcuts to Remote Networks dialog box and clicking Delete.
To remove a shortcut, right-click the shortcut you want to remove in RSWho and select
Remove
. The shortcut will reappear if you rebrowse the original shortcut path and collapse and expand the workstation.
TIP:
If you remove a node containing a network that a shortcut points to, the shortcut will also be removed from
RSWho
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal