Configure a shortcut

  1. From the RSLinx Classic main menu, select
    Communications > Configure Shortcuts
    .
  2. From the
    Configure Shortcuts to Remote Networks
    dialog box, click
    New
    .
  3. In the
    Shortcuts
    pane, type a name for the shortcut (between 1 and 15 characters).
  4. Select the shortcut path using RSWho. The path appears in Shortcut points to this network or chassis as you select it.
  5. Click
    Apply
    to save the new shortcut.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal