ControlNet diagnostic counters

Diagnostic counters are available by right-clicking the processor station in the RSWho window. The available counters are those that are available on the hardware itself. Driver diagnostics are found under the
General
tab in the tabbed dialog box. Driver diagnostics are modeless. If you minimize RSLinx Classic, they can remain on the desktop. The following diagnostic counters are shown with this driver:
Transmitted good
Received good
Total received
Transmitted aborted
Received aborted
Received bad
Update time overload
Blockage
Mismatch events
Unheard occurrences
Out of step events
Network silent
Noise detected
Collisions
Commands received
Channel A errors
Channel B errors
Channel warnings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal