Backup/Restore utility command line support

Mandatory switches
b
Backup
r
Restore
f:path
Is required to a valid path to a rsx file.
Optional switches
I
Ignore .rsx version
c
Create the path to the rsx file when performing a backup.
u
Unconditional restore of a older version of a rsx file when performing a restore.
o
Overwrite existing .rsx files
?
Help on switches
Backup example
Backupcmd –b –f:"c:\program files\rockwell software\rslinx\backup.rsx"
Backupcmd –b –f:"c:\backup\backup.rsx"
Restore example
Backupcmd –r –f:"c:\program files\rockwell software\rslinx\backup.rsx"
Backupcmd –r –f:"c:\backup\backup.rsx"
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal