Add a network
To add a network, perform the following steps:
- From the RSLinx Classic main menu, selectCommunications > Configure Drivers.
- From theConfigure Driversdialog box, double-clickRemote Devices via RSLinx Gatewayfrom theAvailable Driverslist.
- Click theConfigure Browsertab.
- In theNetwork Numberbox, enter the network you want to add and clickAdd. The network you entered appears in theNetworks Currently Selected for Browsing.
- ClickApply.
Provide Feedback