RSLinx Classic for FactoryTalk View
If RSLinx Classic Lite (no activation present) is installed on a machine that has FactoryTalk View SE/ME, it uses FactoryTalk View's license to start as RSLinx Classic for FactoryTalk View. However, please keep in mind that RSLinx Classic for FactoryTalk View:
- in addition to supporting FactoryTalk View SE/ME as OPC clients, supports Data Monitor.
- does not support RSView32, FactoryTalk Transaction Manager, RSTrend, WinView, RSLogix 5/500, Logix Designer application and third-party OPC clients.TIP:In RSLinx Classic v2.53.00 and later, RSLinx Lite enables OPC connectivity for FactoryTalk View SE/ME.
Provide Feedback