Uninstall Device Description File Installation Tool and all EDS files

To Uninstall Device Description File Installation Tool and all EDS files, perform the following steps:
  1. Select
    Start > Rockwell Software > Uninstall Device Description File Installation Tool and all EDS files
    to launch the uninstall EDS subsystem process.
    IMPORTANT:
    If any of the products listed below are installed on your computer, you are not recommended to uninstall the EDS subsystem:
    • RSNetworx
    • RSLinx Classic
    • FactoryTalk Linx
    • RSLogix 5000 or Studio 5000 Logix Designer
    • Logix Designer (RSLogix 5000) Module Profiles
    • FactoryTalk Services Platform
  2. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal