Manually upload and register EDS files of devices in the RSWho

For an online device whose EDS file is not registered, RSLinx Classic detects whether the device contains an EDS file within its firmware. If there is an EDS file found, you can manually upload and register the EDS file in the
RSWho
.
To manually upload and register DES files from device in the
RSWho
, perform the following steps:
  1. Connect the device to the computer.
  2. Open RSLinx Classic, and then browse for the device in the
    RSWho
    .
  3. Once you find the device, right-click it, and select
    Upload EDS file from device
    from the context menu.
TIP:
If you right-click an unregistered online device, and the context menu does not contain the
Upload EDS file from device
option, it means the device does not support this function.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal