EDS Service component did not register properly
While installing RSLinx Classic, or running the Device Description File Installation Tool, you:
- Encounter an error message, “Our EDS Services component did not register properly. Contact Rockwell Software Support for Assistance,” and
- Notice that all the control buttons the Device Description File Installation Tool are not available, as well as
- Notice that the device icons in RSWho appear as globesIt indicates that the file RSEDS.DLL did not register properly. To correct the problem, perform the following steps:
- Ensure that RSEDS.DLL exists, and register it using the REGSVR32.
- Reboot your computer to run the Device Description File Installation Tool to register the EDS files directory on the computer.
Provide Feedback