Troubleshooting installation

If RSLinx Classic does not start or run properly, consider the following:
  • Does your computer have enough memory? Running RSLinx Classic requires a minimum of 4 GB of RAM.
  • Does your computer have enough disk space? Running RSLinx Classic requires a minimum of 2.2 GB of available hard disk space.
  • Do you have the correct version of RSLinx Classic installed? If your RSLinx Classic installation shows as RSLinx Classic Lite, RSLinx Classic Single Node, or RSLinx Classic OEM, the proper activation files are not installed. From within RSLinx Classic, select
    Help > About RSLinx Classic
    to view information about activation files.
  • Have you reinstalled an earlier Service Pack or removed a component, such as DCOM, that RSLinx Classic requires?
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal