Select default DDE project

  1. Select
    File > Select Default Project
    from the RSLinx Classic main menu.
  2. From the
    Select Default DDE Project
    dialog box, select the DDE project to open from the current DDE projects list.
  3. Click
    OK
    .
  4. When you select a default DDE project, that project becomes the active project when you start RSLinx Classic, regardless of the project you last edited. If you have not created a project, a Default project is automatically created and selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal