Open project
- SelectFile > Open Projectfrom the RSLinx Classic main menu.
- From the Open DDE Project dialog box, select the DDE project to open from the Currently Defined Projects list.
- ClickOK.
If you have DDE connections open to RSLinx Classic and select the Open Project menu item, the following message displays:
"Cannot change projects while DDE connections are active to RSLinx Classic. Please close all DDE connections to continue."
Provide Feedback