Configure an OPC client to obtain data from a processor using an alias topic

To configure an OPC client to obtain data from a processor using an alias topic, perform the following steps:
  1. Using one of the real topics associated with the alias topic, browse the target processor to collect names of the OPC Items.
  2. Once collected, add the OPC Items to be used in the OPC client.
  3. From the OPC client, export the tag database to a text file.
  4. Open the text file, and replace the topic name with the alias topic name.
  5. Save the text file, and import it into the OPC client tag database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal