SLC on DH Plus diagnostic counters

Diagnostic counters are available by right-clicking the processor station in the RSWho window. The available counters are those that are available on the hardware itself. Driver diagnostics are found under the General tab in the tabbed dialog. Driver diagnostics are modeless; therefore, they can remain on the desktop if you minimize RSLinx Classic. The following diagnostic counters are shown with this driver:
Messages received successfully
Transmit messages
Receive bad messages
Transmit bad messages
Queue errors
Link dead timeout
Token claim won
Token claim lost
SOL success
Token retrys
Token fails
Token start scan
SOL scan failed
Duplicate nodes
Dropped node
SDA message received
Received bad packet
Retransmissions
Buffer not armed
LSAP was off
SDA OK
NAKs sent
SDA ACK timeout
NAKs received
SDA retries low byte
Other retries
Destination has no buffers
Destination bad lsap
SDN failed
SOL Rotation
SDN received
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal