Optimized packet states
State | Description |
|---|---|
Unknown | Should never occur. |
Initialized | Occurs when the optimized packet is created, before it is sent to the ControlLogix. |
Creating Connection | Indicates that a connection to the ControlLogix must be created, and then an optimized packet must be created. |
Creating Optimized Packet | Indicates that an optimized packet is being created in the ControlLogix. |
Add_Remove_Read | Normal state when reading, adding items, or removing items. If adding or removing items, the following two states should be appended. |
Adding Items | Indicates the ControlLogix is in the process of adding items during Add_Remove_Read. |
Removing Items | Indicates the ControlLogix is in the process of removing items during Add_Remove_Read. |
Read Pending | Indicates there is a packet with a pending request for the ControlLogix. |
Remove Optimized Packet | Instructs the ControlLogix to remove the optimized packet. |
Closing Connection | Closes an unnecessary connection. |
Removed | Indicates the packet has been removed from ControlLogix but not yet destroyed. |
Program being downloaded | Indicates a program is being downloaded. The ControlLogix optimized packets will not be recreated until the upload is complete. |
Unsolicited Packet | Indicates this is an unsolicited packet that is not sent to the controller. |
Provide Feedback