Block read sizes

To read more than one value at a time, use a block read command format by adding length and format specifiers (see Generic item format). For this to work, you must know the single block maximum size limit. This size limitation is determined by the maximum quantity of bytes that can be moved within a single Data Highway packet, and varies based on which device generated the packet. If you are using polled mode, RSLinx Classic generates the packet. If you are using unsolicited mode, the processor generates the packet.
The maximum size is based on the maximum number of bytes that can be moved within a single Data Highway packet, and, when a request for data is made,
all
the members of the data table element being retrieved. For example, if requesting
T4:0.ACC
, a request is actually made for
T4:0
(Control word),
T4:0.PRE
, and
T4:0.ACC
. Therefore, it requests the accumulated value, as well as the control and preset values.
When determining the maximum number of elements to be read within a single block, consider both the maximum quantity of bytes that can be moved and the number of words within a single element. These values vary with both the originator of the data movement command and the type of data. For both polled and unsolicited mode, RSLinx Classic refuses the data request if the block size entered into the address field exceeds the maximum mode value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal