PIUNSOL.INI file format

PIUNSOL.INI consists of a series of entries, one for each 5820-EI module RSLinx Classic will register with for unsolicited messages. For example:
[130.151.188.135]
0200=4
010070=16
where
[130.151.188.135]
is the IP address of the 5820-EI
0200
is the first PLC-2 memory address to register and 4 is the length of that memory address
010070
is the second PLC-2 memory address to register and 16 is the length of that memory address
Address is expressed in octal and length is expressed in decimal. The examples show the common leading 0 just for convenience. Notice that the same PLC-2 memory address/length pair can appear in multiple hostname entries.
To send data to a DDE client, create a DDE topic that points to the PLC-5 sending the message, but define the PLC topic type as a PLC-2. The DDE item defined in the client is the PLC-2 address defined in PIUNSOL.INI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal