Write a block

The following program reads five user-inputted numbers located in five text boxes (named
txtBlock1-txtBlock5
). The necessary DDE string is then constructed, stored in the text property of a text box with the name of
txtPokebox
, and sent to RSLinx Classic. This program is performed once the
Command1
button (Write Block) is clicked.
Sub Command1_Click ()
tab1 = Chr$(9)
'Define tab1 as TAB (ANSI code for TAB = 9)
The following line strings the data together with a Tab separating the numbers
txtPokebox.Text = txtBlock1.Text & tab1 & txtBlock2.Text & tab1 & txtBlock3.Text & tab1 & txtBlock4.Text & tab1 & txtBlock5.Text
txtPokebox.LinkTopic = "RSLinx|testsol"
'Define DDE application and Topic
txtPokebox.LinkItem = "N7:0,L5"
'Define DDE link item
txtPokebox.LinkMode = 2
'Open DDE link (manual)
txtPokebox.LinkPoke
'Write data to RSLinx
txtPokebox.LinkMode = 0
'Close DDE link
End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal