Microsoft Excel DDE via VBA examples
One way to accomplish a DDE write in Excel is through the use of Excel macros, which are DDE cold links. All functions used in these macros are Microsoft Excel standards and are explained in detail in the Microsoft Excel 5 Worksheet Function Reference. The following are four examples using RSLinx Classic with Excel macros:
Provide Feedback