Communication Events

Select
DDE/OPC > Communication Events
to display information about DDE/OPC error messages logged while running RSLinx Classic with DDE/OPC compliant programs. Each time an error message is seen by RSLinx Classic, the number of errors logged counter is increased by one and the entry is added to the window viewer.
For a more detailed look at the information concerning the logged error, click the message in the window viewer and look at the information added to the
Selected Error Details
section near the bottom of the dialog box. Communication events displays details such as processor manufacturer and type, the item affected by the error, and the DDE/OPC command type of the message.
To enable logging of DDE errors, select
DDE/OPC > Options
and select the
Log Communication Errors
check box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal