CIP Diagnostics
The CIP Diagnostics dialog provides global information that is not specific to any driver. This dialog is modeless (like Driver Diagnostics), and remains on the desktop if you minimize RSLinx Classic. The
CIP Diagnostics
dialog currently opens CIP Dispatching, Messaging, and CIP Connections diagnostics. Diagnostic counters shown are only available in this dialog, and are not available via RSWho
.Provide Feedback