What is an "activation file?"

An activation file is a digitally signed, plain-text file that activates a software product and “locks” the activation to a particular piece of hardware, such as a computer’s hard disk or Ethernet card. The contents of an activation file are protected by a signature, generated by Rockwell Software, which is based on machine-specific information that you provide when you install the software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal