Grace period
In RSLinx Classic version 2.52.00 (CPR 9) and later, the software supports a seven-day
activation grace period when a valid activation is not found. During grace period:
- When the software is started, a message is logged to the FactoryTalk Diagnostic log every four hours until a valid activation is found.
- RSLinx Classic can be started an unlimited number of times. If the grace period ends and a valid activation is not found, RSLinx Classic Lite is started.TIP:If RSLinx Classic does not successfully obtain valid activations (for example, a network failure occurs), the software attempts to run in grace period for up to seven days.
For more information on the FactoryTalk Activation Manager grace period, see
FactoryTalk Activation Manager Help
.Provide Feedback