Activate RSLinx Classic in Installation Setup Wizard
RSLinx Classic version 3.70.00 and later supports to activate the software during the
software installation. The RSLinx Classic Installation Setup Wizard (version 3.70.00 and
later) contains an
Activate products using FactoryTalk Activation
check box. This no
longer requires you to open FactoryTalk Activation Manager to activate the software. If you
select the checkbox, a Software Activation
dialog opens. Complete the following
steps:- Enter the serial number and product key from your Activation Certificate.
- SelectActivate locallyto activate RSLinx Classic on a single computer, or selectActivate using a dongleto activate RSLinx Classic on any computer by using a dongle.TIP:TheActivate using a dongleoption requires that you have a dongle to lock the activation.
- ClickContinue.
You can still activate RSLinx Classic via FactoryTalk Activation Manager by clicking the
Explore other options
link in the Software Activation
dialog box. The link provides direct access to the FactoryTalk Activation Manager. For steps to activate RSLinx Classic in FactoryTalk Activation Manager software, see Activate RSLinx Classic using FactoryTalk Activation Manager.Provide Feedback